DC-DC power
converters for
industrial applications
DC-DC Converters make it possible to integrate storage systems into the drive line-up. Example: regenerative energy can be stored temporarily and then used for the process as required. The stored energy can also be supplied to the drive line-up in the event of peak load requirements or power failures. Siemens offers DC-DC Converters from the SINAMICS product family for these applications.
![Key visual DC DC Converter DC DC Power Converter - Key visual](https://assets.new.siemens.com/siemens/assets/api/uuid:697c1b0a-dc8e-41fe-ab24-bf5933db782c/width:100/quality:low/DC-DC-Power-Converter-Key-visual.png)
DC-DC Converters make it possible to integrate storage systems into the drive line-up. Example: regenerative energy can be stored temporarily and then used for the process as required. The stored energy can also be supplied to the drive line-up in the event of peak load requirements or power failures. Siemens offers DC-DC Converters from the SINAMICS product family for these applications.