Ctrl-E: The checklist for energy efficiency

Saving energy in machine tool use has been a concern of ours for a long time. The "Ctrl-Energy" function was introduced in SINUMERIK back in 2012: Since then, the key combination Ctrl-E has provided standardized access to energy-saving functions of SINUMERIK Operate and the machine tool. What benefits can be achieved with this in practice? This checklist provides answers.

Ftoo: Ctrl-E-Eingabe auf dem Tastenfeld einer SINUMERIK CNC

Saving energy in machine tool use has been a concern of ours for a long time. The "Ctrl-Energy" function was introduced in SINUMERIK back in 2012: Since then, the key combination Ctrl-E has provided standardized access to energy-saving functions of SINUMERIK Operate and the machine tool. What benefits can be achieved with this in practice? This checklist provides answers.