Transformer differential protection
The SIPROTEC 7UT82/85/86/87 transformer differential protection have been designed specifically for the protection of two and multi-winding (up to 5 sides). transformers. They are the main protection for the transformer and contain many other protection and monitoring functions. The additional protection functions can also be used as backup protection for subsequent protected objects (such as cabl…
![Transformer differential protection Transformer differential protection](https://assets.new.siemens.com/siemens/assets/api/uuid:1a8da1ecb1c6401c3d4ac155234daf31b9004104/width:100/quality:low/1a8da1ecb1c6401c3d4ac155234daf31b9004104.jpg)
The SIPROTEC 7UT82/85/86/87 transformer differential protection have been designed specifically for the protection of two and multi-winding (up to 5 sides). transformers. They are the main protection for the transformer and contain many other protection and monitoring functions. The additional protection functions can also be used as backup protection for subsequent protected objects (such as cabl…