SINUMERIK – Production with a focus on energy efficiency

With resources being scarce, "achieving more with less" is the order of the day. Legislators around the globe – especially in the European Union – are tough when it comes to sustainability. The extent to which companies are impacted can be seen in how contracts are awarded in the public domain. This is reflected in the fact that almost all large industrial corporations have made CO2 neutrality one…
CNC4you
With resources being scarce, "achieving more with less" is the order of the day. Legislators around the globe – especially in the European Union – are tough when it comes to sustainability. The extent to which companies are impacted can be seen in how contracts are awarded in the public domain. This is reflected in the fact that almost all large industrial corporations have made CO2 neutrality one…