Digital twins for CNC job preparation

A machine tool is at its most productive when it is producing chips. Activities that lead to unproductive machine times should therefore be consistently transferred to CNC job preparation. Besides CNC programming, which is often still performed with the machine's protective doors open, these are also the times for testing and running in the programs.
A machine tool is at its most productive when it is producing chips. Activities that lead to unproductive machine times should therefore be consistently transferred to CNC job preparation. Besides CNC programming, which is often still performed with the machine's protective doors open, these are also the times for testing and running in the programs.