Connection capacity halved with sustainable UltraCap

UltraCaps can briefly store and release energy. This allows companies to save energy and limit their required connection capacity, making them less dependent on the capacity and stability of the energy grid. Torsit Hijsinstallaties applied Siemens UltraCaps for the first time in the Netherlands. As a result, two warehouse cranes can now operate on a 16 A connection verses a 32 A connection.
Key Visual Reference Torsit
UltraCaps can briefly store and release energy. This allows companies to save energy and limit their required connection capacity, making them less dependent on the capacity and stability of the energy grid. Torsit Hijsinstallaties applied Siemens UltraCaps for the first time in the Netherlands. As a result, two warehouse cranes can now operate on a 16 A connection verses a 32 A connection.